CR
ID |
Headline |
ENGR139327 |
Multi-Touch:
HSD100 Multi-finger Touch is not easy to use. 100% |
ENGR143606 |
EETI Multi-Touch:
Unexpected successfully drawing lines in Touch D4 mode.100% |
ENGR143644 |
EETI Multi-Touch
error after system suspend/resume. Possibility 100% |
ENGR143700 |
Fake battery should report fully
charged battery. |
ENGR143720 |
PowerKey: The time setting of pressing
"power" key to bring power transition from full on to power off
doesn't correspond with SRS.100% |
ENGR143962 |
PP and PRP IC
flip issue |
ENGR138523 |
MX53 DDR3 platform has screen flicker
issue when play two VGA video on XGA panel. |
ENGR139745 |
HDMI: Audio
output from SPDIF to HDMI is not stable for some streams. 100% |
ENGR140570 |
Onkey/OTP PIMC
boards: Suspend will auto-resume if connented USB mouse to OTG port |
ENGR140652 |
OTP PIMC boards:
SPDIF output lost after supend/resume twice. |
ENGR141409 |
The second overlay can't be enabled
after resolution change. |
ENGR142363 |
Data abort and hang on WEC 7 |
ENGR142680 |
SDHC: it failed to handle power
operation correctly. |
ENGR142972 |
[GPU] Mismatch
between function prototype and call |
ENGR142974 |
Minipci-e wifi:
wifi not working after suspend & resume. |
|
|